How to add FreeRTOS for s32k344 in S32 DS 3.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add FreeRTOS for s32k344 in S32 DS 3.4

1,277 Views
tommy1231
Contributor II

I'm working on porting a project from the K1 to the K3 processor.  FOr the K1 the S32 DS has the ability to add FreeRTOS but it is not available for the K3.  I have the RTD installed so the drivers are there for the peripherals but the OS is blank when I go to the manage SDKs window.  I'm guessing I have to installed an additional package but I did not see anything in the software portal.

tommy1231_0-1633791569849.png

 

0 Kudos
Reply
0 Replies