How many UARTs can be emulated using FlexIO in S32K144?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How many UARTs can be emulated using FlexIO in S32K144?

1,503 次查看
prasanna_rawke
Contributor II

S32K144 has a option to configure 8 pins as FlexIO data pins. On the other hand, it has 4 shifters and 4 timers as per the datasheet.

And one FlexIO UART TX requires, one shifter and one timer for the operation.

--------------------------------------------------------------------------------------------------------------------

Does it mean that we can emulate only two duplex UARTs (Rx+Tx) using FlexIO?

Is there any way to implement 4 UARTs using FlexIO? For example, in my application, I can keep the baudrate of all UARTs same, which can reduce the number of timers required.

Regards,

Prasanna

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,428 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Prasanna,

As you write, the FlexIO has available 4 Timers, 4 Shifters, 8 Pins

For one UART (TX + RX) 2 shifters and 2 timers are needed.
So, we can configure max 2x UART by FlexIO.

There is a possibility to have several shifters clocked by the same timer but still, we have only 4 shifters.

However, the S32K144 has 3x LPUART, you could use it.

I hope it helps.

Best regards,

Diana

0 项奖励
回复

1,428 次查看
prasanna_rawke
Contributor II

Hello Diana,

Thanks for the clarification.

Actually in my application, all the LPUARTs are already consumed by other modules, and I was going by the impression that 8 FlexIO data pins will cater 4 additional UARTs.

Thanks,

Prasanna

0 项奖励
回复