How many S32K314 FlexCAN PE clocks are there?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How many S32K314 FlexCAN PE clocks are there?

跳至解决方案
1,106 次查看
malove
Contributor IV

Hello.

I am leaving an inquiry because I have questions about the S32K3xx Clock-related documents.

 

studyseok8466_1-1729140794533.png

studyseok8466_2-1729140818389.png

Looking at Figure 59. Other clocks and Table 476 FlexCAN configuration and instances, it says that S32K314 can use a total of 6 FlexCAN instances (FlexCAN0, 1, 2, 3, 4, 5, 6).

 

studyseok8466_0-1729140539838.png

However, looking at Figure 65, FlexCAN[3]_PE_CLK can only use S32K322, S32K341, and S32K342.

So, is there a total of 5 PE clocks and 6 instances supplied to FlexCAN of S32K314?

 

标记 (3)
0 项奖励
回复
1 解答
1,085 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

a note on Fig65 says that from set of three PE clocks (FlexCAN[3:5]_PE_CLK) just a single one (FlexCAN[3]_PE_CLK) is available on S32K322, S32K341 and S32K342 devices. That is because S32K322, S32K341 and S32K342. includes four FlexCAN instances (0-3).
S32K344, S32K324, S32K314 includes six FlexCAN instances and so there are six PE clocks.

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,086 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

a note on Fig65 says that from set of three PE clocks (FlexCAN[3:5]_PE_CLK) just a single one (FlexCAN[3]_PE_CLK) is available on S32K322, S32K341 and S32K342 devices. That is because S32K322, S32K341 and S32K342. includes four FlexCAN instances (0-3).
S32K344, S32K324, S32K314 includes six FlexCAN instances and so there are six PE clocks.

BR, Petr

0 项奖励
回复
1,071 次查看
malove
Contributor IV

thank you I interpreted it wrong. 

0 项奖励
回复