How is the Doze mode working in S32K series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How is the Doze mode working in S32K series

Jump to solution
2,569 Views
176211901
Contributor I

how dose the Doze mode working in S32K series peripheral?

I see the Doze mode in S32K reference manual, but I didn't see the details that how it is working.

Tags (1)
0 Kudos
Reply
1 Solution
2,421 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi wang jian

DOZE mode can optionally keeps peripheral on or off, in Low Power modes. In this way, for example, communication peripheral (LPSPI, LPUART, etc) allow the application to receive data while core is in low power mode.

For your reference please check this link:

Low power and Doze Mode question in S32K 

 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,422 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi wang jian

DOZE mode can optionally keeps peripheral on or off, in Low Power modes. In this way, for example, communication peripheral (LPSPI, LPUART, etc) allow the application to receive data while core is in low power mode.

For your reference please check this link:

Low power and Doze Mode question in S32K 

 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply
2,421 Views
176211901
Contributor I

Thanks for your reply.

There is a another question:

what is the difference between DOZEN and MEN in LPSPI Control Register ?

 

0 Kudos
Reply