How generate digital signal in s32k144evb?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How generate digital signal in s32k144evb?

1,498 次查看
miketorres
Contributor II

I have to do program. One of the tasks is write function which generate digital signal about 100hz (square signal). I have to use only pin with gpio function.Do you have any sugestion or similar code which do something like this?

0 项奖励
回复
3 回复数

1,466 次查看
miketorres
Contributor II

@Senlent  Thank you very much, I did it and it works. Could you help me with last function in this program? Maybe you know how can I do it?

https://community.nxp.com/t5/S32K/How-can-I-send-signal-value-in-Hz-in-fixed-time-interval-1s/m-p/13...

0 项奖励
回复

1,457 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@miketorres

        Glad to see you solved the problem !

        I saw that my colleague has already started answering your new question, and he will help you solve it.

BR!

     Jim,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,475 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@miketorres

              Already replied to you under another similar topic of yours

BR!

      Jim,