How do I set a pin of S32K344 to open drain output mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I set a pin of S32K344 to open drain output mode

ソリューションへジャンプ
1,249件の閲覧回数
SCoder41
Contributor III

How do I set a pin of S32K344 to open drain output mode.We have designed the hardware to be in an open drain output triggered mode, with a 5V pull-up,Our hardware schematic is shown in the following figure

7.png

0 件の賞賛
返信
1 解決策
1,212件の閲覧回数
PavelL
NXP Employee
NXP Employee

Hello @SCoder41 ,

important is RTD version. If you look to the link in the first reply, there is function 

void Siul2_Port_Ip_SetPinDirection(Siul2_Port_Ip_PortType * const base, uint16 pin, Siul2_Port_Ip_PortDirectionType direction);

which can help you.

Best regards,

Pavel

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
1,236件の閲覧回数
PavelL
NXP Employee
NXP Employee

Hello @SCoder41 ,

there's no "true" open drain support on S32K344 (GPIO open drain? - NXP Community). But your application doesn't look like time critical (many MHz), so you can manage open drain mode easily by switching GPIO between "HighZ" mode and "ouput low" mode.

Best regards,

Pavel

0 件の賞賛
返信
1,219件の閲覧回数
SCoder41
Contributor III
S32DS3.5
0 件の賞賛
返信
1,223件の閲覧回数
SCoder41
Contributor III
How to set GPIO to "HighZ" mode
0 件の賞賛
返信
1,213件の閲覧回数
PavelL
NXP Employee
NXP Employee

Hello @SCoder41 ,

important is RTD version. If you look to the link in the first reply, there is function 

void Siul2_Port_Ip_SetPinDirection(Siul2_Port_Ip_PortType * const base, uint16 pin, Siul2_Port_Ip_PortDirectionType direction);

which can help you.

Best regards,

Pavel

0 件の賞賛
返信
1,144件の閲覧回数
SCoder41
Contributor III
Which address should the first parameter of the function 'Siu l2 Port Ip_SetPinDirection' point to?
0 件の賞賛
返信
1,137件の閲覧回数
PavelL
NXP Employee
NXP Employee

Hello @SCoder41 ,

here's example for PTG29:

#include "Siul2_Port_Ip.h"

Siul2_Port_Ip_SetPinDirection(PORTG_H_HALF, 29-16, SIUL2_PORT_HI_Z);

16 shall be subtracted for the upper half port numbers.

Best regards,

Pavel

0 件の賞賛
返信