How do I link EB Tresos to the S32K3 RTD Drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I link EB Tresos to the S32K3 RTD Drivers

Jump to solution
1,400 Views
Andy_B
Contributor I

How do I link the S32K3 RTD drivers to EB Tresos?  I've had to re-install S32, and I can't find the step where it asks for the path to EB Tresos.  Thanks in advance for any insight.

Tags (1)
0 Kudos
Reply
1 Solution
1,393 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Andy_B,

If you want to use the S32K3 RTD with EB Tresos, please install latest SW32K3_RTD_4.4_2.0.2_D2211.exe.  During installation, you can select EB Tresos install directory. Then you should be able to see the link:

install SW32K3_RTD_4.4_2.0.2_D2211.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,394 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Andy_B,

If you want to use the S32K3 RTD with EB Tresos, please install latest SW32K3_RTD_4.4_2.0.2_D2211.exe.  During installation, you can select EB Tresos install directory. Then you should be able to see the link:

install SW32K3_RTD_4.4_2.0.2_D2211.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply