How can I set :HEAP_SIZE ; STACK_SIZE ;M_VECTOR_RAM_SIZE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I set :HEAP_SIZE ; STACK_SIZE ;M_VECTOR_RAM_SIZE

Jump to solution
2,095 Views
jingfang
Contributor IV

How can I set :HEAP_SIZE ; STACK_SIZE ;M_VECTOR_RAM_SIZE?

How about range?

0 Kudos
Reply
1 Solution
2,072 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @jingfang 

To be in the same context I am going to take as a reference the attached which is a structure of a linker file from an SDK example.

The size of the bss, stack and heap are taken concerning memory space in m_data_2(SRAM_U). So sizes are theoretically limited by available SRAM memory. 

Regarding, the vector ram size is taken concerning memory space in m_data(SRAM_L), but unlike the previous one, in this one, there is also data ram and code ram.

You also could try to use the m_data section for heap and stack, but you would need to corroborate that you have still memory space in this section.

/*
** ###################################################################
**     Processor:           S32K144 with 64 KB SRAM
**     Compiler:            GNU C Compiler
**
**     Abstract:
**         Linker file for the GNU C Compiler
**
**     Copyright (c) 2015-2016 Freescale Semiconductor, Inc.
**     Copyright 2017-2018 NXP
**     All rights reserved.
**
**     NXP Confidential. This software is owned or controlled by NXP and may only be
**     used strictly in accordance with the applicable license terms. By expressly
**     accepting such terms or by downloading, installing, activating and/or otherwise
**     using the software, you are agreeing that you have read, and that you agree to
**     comply with and are bound by, such license terms. If you do not agree to be
**     bound by the applicable license terms, then you may not retain, install,
**     activate or otherwise use the software. The production use license in
**     Section 2.3 is expressly granted for this software.
**
**     http:                 www.nxp.com
** ###################################################################
*/

/* Entry Point */
ENTRY(Reset_Handler)

HEAP_SIZE  = DEFINED(__heap_size__)  ? __heap_size__  : 0x00000400;
STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x00000400;

/* If symbol __flash_vector_table__=1 is defined at link time
 * the interrupt vector will not be copied to RAM.
 * Warning: Using the interrupt vector from Flash will not allow
 * INT_SYS_InstallHandler because the section is Read Only.
 */
M_VECTOR_RAM_SIZE = DEFINED(__flash_vector_table__) ? 0x0 : 0x0400;

/* Specify the memory areas */
MEMORY
{
  /* Flash */
  m_interrupts          (RX)  : ORIGIN = 0x00000000, LENGTH = 0x00000400
  m_flash_config        (RX)  : ORIGIN = 0x00000400, LENGTH = 0x00000010
  m_text                (RX)  : ORIGIN = 0x00000410, LENGTH = 0x0007FBF0

  /* SRAM_L */
  m_data                (RW)  : ORIGIN = 0x1FFF8000, LENGTH = 0x00008000

  /* SRAM_U */
  m_data_2              (RW)  : ORIGIN = 0x20000000, LENGTH = 0x00007000
}

/* Define output sections */
SECTIONS
{
  /* The startup code goes first into internal flash */
  .interrupts :
  {
    __VECTOR_TABLE = .;
    __interrupts_start__ = .;
    . = ALIGN(4);
    KEEP(*(.isr_vector))     /* Startup code */
    __interrupts_end__ = .;
    . = ALIGN(4);
  } > m_interrupts

  .flash_config :
  {
    . = ALIGN(4);
    KEEP(*(.FlashConfig))    /* Flash Configuration Field (FCF) */
    . = ALIGN(4);
  } > m_flash_config

  /* The program code and other data goes into internal flash */
  .text :
  {
    . = ALIGN(4);
    *(.text)                 /* .text sections (code) */
    *(.text*)                /* .text* sections (code) */
    *(.rodata)               /* .rodata sections (constants, strings, etc.) */
    *(.rodata*)              /* .rodata* sections (constants, strings, etc.) */
    *(.init)                 /* section used in crti.o files */
    *(.fini)                 /* section used in crti.o files */
    *(.eh_frame)             /* section used in crtbegin.o files */
    . = ALIGN(4);
  } > m_text

  /* Section used by the libgcc.a library for fvp4 */
  .ARM :
  {
    __exidx_start = .;
    *(.ARM.exidx*)
    __exidx_end = .;
  } > m_text

  __etext = .;    /* Define a global symbol at end of code. */
  __DATA_ROM = .; /* Symbol is used by startup for data initialization. */

  .interrupts_ram :
  {
    . = ALIGN(4);
    __VECTOR_RAM__ = .;
    __RAM_START = .;
    __interrupts_ram_start__ = .; /* Create a global symbol at data start. */
    *(.m_interrupts_ram)          /* This is a user defined section. */
    . += M_VECTOR_RAM_SIZE;
    . = ALIGN(4);
    __interrupts_ram_end__ = .;   /* Define a global symbol at data end. */
  } > m_data

  __VECTOR_RAM = DEFINED(__flash_vector_table__) ? ORIGIN(m_interrupts) : __VECTOR_RAM__ ;
  __RAM_VECTOR_TABLE_SIZE = DEFINED(__flash_vector_table__) ? 0x0 : (__interrupts_ram_end__ - __interrupts_ram_start__) ;

  .data : AT(__DATA_ROM)
  {
    . = ALIGN(4);
    __DATA_RAM = .;
    __data_start__ = .;      /* Create a global symbol at data start. */
    *(.data)                 /* .data sections */
    *(.data*)                /* .data* sections */
    . = ALIGN(4);
    __data_end__ = .;        /* Define a global symbol at data end. */
  } > m_data

  __DATA_END = __DATA_ROM + (__data_end__ - __data_start__);
  __CODE_ROM = __DATA_END; /* Symbol is used by code initialization. */

  .code : AT(__CODE_ROM)
  {
    . = ALIGN(4);
    __CODE_RAM = .;
    __code_start__ = .;      /* Create a global symbol at code start. */
    __code_ram_start__ = .;
    *(.code_ram)             /* Custom section for storing code in RAM */
    . = ALIGN(4);
    __code_end__ = .;        /* Define a global symbol at code end. */
    __code_ram_end__ = .;
  } > m_data

  __CODE_END = __CODE_ROM + (__code_end__ - __code_start__);
  __CUSTOM_ROM = __CODE_END;

  /* Custom Section Block that can be used to place data at absolute address. */
  /* Use __attribute__((section (".customSection"))) to place data here. */
  .customSectionBlock  ORIGIN(m_data_2) : AT(__CUSTOM_ROM)
  {
    __customSection_start__ = .;
    KEEP(*(.customSection))  /* Keep section even if not referenced. */
    __customSection_end__ = .;
  } > m_data_2
  __CUSTOM_END = __CUSTOM_ROM + (__customSection_end__ - __customSection_start__);
  __rom_end    = __CUSTOM_END;

  /* Uninitialized data section. */
  .bss :
  {
    /* This is used by the startup in order to initialize the .bss section. */
    . = ALIGN(4);
    __BSS_START = .;
    __bss_start__ = .;
    *(.bss)
    *(.bss*)
    *(COMMON)
    . = ALIGN(4);
    __bss_end__ = .;
    __BSS_END = .;
  } > m_data_2

   /* Put heap section after the program data */
  .heap :
  {
    . = ALIGN(8);
    __end__ = .;
    __heap_start__ = .;
    PROVIDE(end = .);
    PROVIDE(_end = .);
    PROVIDE(__end = .);
    __HeapBase = .;
    . += HEAP_SIZE;
    __HeapLimit = .;
    __heap_limit = .;
    __heap_end__ = .;
  } > m_data_2

  /* Initializes stack on the end of block */
  __StackTop   = ORIGIN(m_data_2) + LENGTH(m_data_2);
  __StackLimit = __StackTop - STACK_SIZE;
  PROVIDE(__stack = __StackTop);
  __RAM_END = __StackTop;

  .stack __StackLimit :
  {
    . = ALIGN(8);
    __stack_start__ = .;
    . += STACK_SIZE;
    __stack_end__ = .;
  } > m_data_2

  .ARM.attributes 0 : { *(.ARM.attributes) }
  
  /* Memory validation */
  ASSERT(__rom_end <= (ORIGIN(m_text) + LENGTH(m_text)), "Region m_text overflowed!")

  ASSERT(__StackLimit >= __HeapLimit, "region m_data_2 overflowed with stack and heap")
}

 

View solution in original post

0 Kudos
Reply
3 Replies
2,087 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @jingfang 

Witch MCU are you using?

Let me suggest to you take a look at the linker files of the example projects for S32K1 and S32K3, there you are going to be able to find how these are set.

Also, the range depends on the memory.

 

B.R.

VaneB

0 Kudos
Reply
2,079 Views
jingfang
Contributor IV

S32K144,how should be respond?

jingfang_0-1681970747701.png

 

0 Kudos
Reply
2,073 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @jingfang 

To be in the same context I am going to take as a reference the attached which is a structure of a linker file from an SDK example.

The size of the bss, stack and heap are taken concerning memory space in m_data_2(SRAM_U). So sizes are theoretically limited by available SRAM memory. 

Regarding, the vector ram size is taken concerning memory space in m_data(SRAM_L), but unlike the previous one, in this one, there is also data ram and code ram.

You also could try to use the m_data section for heap and stack, but you would need to corroborate that you have still memory space in this section.

/*
** ###################################################################
**     Processor:           S32K144 with 64 KB SRAM
**     Compiler:            GNU C Compiler
**
**     Abstract:
**         Linker file for the GNU C Compiler
**
**     Copyright (c) 2015-2016 Freescale Semiconductor, Inc.
**     Copyright 2017-2018 NXP
**     All rights reserved.
**
**     NXP Confidential. This software is owned or controlled by NXP and may only be
**     used strictly in accordance with the applicable license terms. By expressly
**     accepting such terms or by downloading, installing, activating and/or otherwise
**     using the software, you are agreeing that you have read, and that you agree to
**     comply with and are bound by, such license terms. If you do not agree to be
**     bound by the applicable license terms, then you may not retain, install,
**     activate or otherwise use the software. The production use license in
**     Section 2.3 is expressly granted for this software.
**
**     http:                 www.nxp.com
** ###################################################################
*/

/* Entry Point */
ENTRY(Reset_Handler)

HEAP_SIZE  = DEFINED(__heap_size__)  ? __heap_size__  : 0x00000400;
STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x00000400;

/* If symbol __flash_vector_table__=1 is defined at link time
 * the interrupt vector will not be copied to RAM.
 * Warning: Using the interrupt vector from Flash will not allow
 * INT_SYS_InstallHandler because the section is Read Only.
 */
M_VECTOR_RAM_SIZE = DEFINED(__flash_vector_table__) ? 0x0 : 0x0400;

/* Specify the memory areas */
MEMORY
{
  /* Flash */
  m_interrupts          (RX)  : ORIGIN = 0x00000000, LENGTH = 0x00000400
  m_flash_config        (RX)  : ORIGIN = 0x00000400, LENGTH = 0x00000010
  m_text                (RX)  : ORIGIN = 0x00000410, LENGTH = 0x0007FBF0

  /* SRAM_L */
  m_data                (RW)  : ORIGIN = 0x1FFF8000, LENGTH = 0x00008000

  /* SRAM_U */
  m_data_2              (RW)  : ORIGIN = 0x20000000, LENGTH = 0x00007000
}

/* Define output sections */
SECTIONS
{
  /* The startup code goes first into internal flash */
  .interrupts :
  {
    __VECTOR_TABLE = .;
    __interrupts_start__ = .;
    . = ALIGN(4);
    KEEP(*(.isr_vector))     /* Startup code */
    __interrupts_end__ = .;
    . = ALIGN(4);
  } > m_interrupts

  .flash_config :
  {
    . = ALIGN(4);
    KEEP(*(.FlashConfig))    /* Flash Configuration Field (FCF) */
    . = ALIGN(4);
  } > m_flash_config

  /* The program code and other data goes into internal flash */
  .text :
  {
    . = ALIGN(4);
    *(.text)                 /* .text sections (code) */
    *(.text*)                /* .text* sections (code) */
    *(.rodata)               /* .rodata sections (constants, strings, etc.) */
    *(.rodata*)              /* .rodata* sections (constants, strings, etc.) */
    *(.init)                 /* section used in crti.o files */
    *(.fini)                 /* section used in crti.o files */
    *(.eh_frame)             /* section used in crtbegin.o files */
    . = ALIGN(4);
  } > m_text

  /* Section used by the libgcc.a library for fvp4 */
  .ARM :
  {
    __exidx_start = .;
    *(.ARM.exidx*)
    __exidx_end = .;
  } > m_text

  __etext = .;    /* Define a global symbol at end of code. */
  __DATA_ROM = .; /* Symbol is used by startup for data initialization. */

  .interrupts_ram :
  {
    . = ALIGN(4);
    __VECTOR_RAM__ = .;
    __RAM_START = .;
    __interrupts_ram_start__ = .; /* Create a global symbol at data start. */
    *(.m_interrupts_ram)          /* This is a user defined section. */
    . += M_VECTOR_RAM_SIZE;
    . = ALIGN(4);
    __interrupts_ram_end__ = .;   /* Define a global symbol at data end. */
  } > m_data

  __VECTOR_RAM = DEFINED(__flash_vector_table__) ? ORIGIN(m_interrupts) : __VECTOR_RAM__ ;
  __RAM_VECTOR_TABLE_SIZE = DEFINED(__flash_vector_table__) ? 0x0 : (__interrupts_ram_end__ - __interrupts_ram_start__) ;

  .data : AT(__DATA_ROM)
  {
    . = ALIGN(4);
    __DATA_RAM = .;
    __data_start__ = .;      /* Create a global symbol at data start. */
    *(.data)                 /* .data sections */
    *(.data*)                /* .data* sections */
    . = ALIGN(4);
    __data_end__ = .;        /* Define a global symbol at data end. */
  } > m_data

  __DATA_END = __DATA_ROM + (__data_end__ - __data_start__);
  __CODE_ROM = __DATA_END; /* Symbol is used by code initialization. */

  .code : AT(__CODE_ROM)
  {
    . = ALIGN(4);
    __CODE_RAM = .;
    __code_start__ = .;      /* Create a global symbol at code start. */
    __code_ram_start__ = .;
    *(.code_ram)             /* Custom section for storing code in RAM */
    . = ALIGN(4);
    __code_end__ = .;        /* Define a global symbol at code end. */
    __code_ram_end__ = .;
  } > m_data

  __CODE_END = __CODE_ROM + (__code_end__ - __code_start__);
  __CUSTOM_ROM = __CODE_END;

  /* Custom Section Block that can be used to place data at absolute address. */
  /* Use __attribute__((section (".customSection"))) to place data here. */
  .customSectionBlock  ORIGIN(m_data_2) : AT(__CUSTOM_ROM)
  {
    __customSection_start__ = .;
    KEEP(*(.customSection))  /* Keep section even if not referenced. */
    __customSection_end__ = .;
  } > m_data_2
  __CUSTOM_END = __CUSTOM_ROM + (__customSection_end__ - __customSection_start__);
  __rom_end    = __CUSTOM_END;

  /* Uninitialized data section. */
  .bss :
  {
    /* This is used by the startup in order to initialize the .bss section. */
    . = ALIGN(4);
    __BSS_START = .;
    __bss_start__ = .;
    *(.bss)
    *(.bss*)
    *(COMMON)
    . = ALIGN(4);
    __bss_end__ = .;
    __BSS_END = .;
  } > m_data_2

   /* Put heap section after the program data */
  .heap :
  {
    . = ALIGN(8);
    __end__ = .;
    __heap_start__ = .;
    PROVIDE(end = .);
    PROVIDE(_end = .);
    PROVIDE(__end = .);
    __HeapBase = .;
    . += HEAP_SIZE;
    __HeapLimit = .;
    __heap_limit = .;
    __heap_end__ = .;
  } > m_data_2

  /* Initializes stack on the end of block */
  __StackTop   = ORIGIN(m_data_2) + LENGTH(m_data_2);
  __StackLimit = __StackTop - STACK_SIZE;
  PROVIDE(__stack = __StackTop);
  __RAM_END = __StackTop;

  .stack __StackLimit :
  {
    . = ALIGN(8);
    __stack_start__ = .;
    . += STACK_SIZE;
    __stack_end__ = .;
  } > m_data_2

  .ARM.attributes 0 : { *(.ARM.attributes) }
  
  /* Memory validation */
  ASSERT(__rom_end <= (ORIGIN(m_text) + LENGTH(m_text)), "Region m_text overflowed!")

  ASSERT(__StackLimit >= __HeapLimit, "region m_data_2 overflowed with stack and heap")
}

 

0 Kudos
Reply