How can I get a base S32DS project with no error for chip S32K344.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I get a base S32DS project with no error for chip S32K344.

439 Views
Zak_wang
Contributor I

The example project under the file"C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2022_03\SW32K3_RTD_4_4_2_0_0_D2203\Can_TS_T40D34M20I0R0\examples\EBT\Can_example_S32K344" need so much header. but the header is not exist,the most of the header are configure file. Or can I get a appnote for integrate a project.

Thanks

Tags (1)
0 Kudos
1 Reply

420 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Zak_wang

the examples in EBT folder runs on EB Tresos Software, 

Senlent_0-1652432521708.png

The examples in the S32DS folder can be run directly on the S32 Design Studio,

Senlent_1-1652432637565.png

you can take a look at the readme.txt file on both folders to know more.

BR!

     Jim,

 

0 Kudos