I want to change the "drive strength enable" from Disabled to n/a in S32K312 under S32DSv3.5.
The reason is I suspect LPSPI0 is not working to validate ISELED functions.
Here is the current pin configuration.
Solved! Go to Solution.
Hello Heedong Lee,
It cannot be changed.
The N/A option is there for the pads that are GPIO-STANDARD like PTA2.
These pads do not have the MSCR[DSE] implemented.
PTC8 is GPIO-STANDARD-PLUS where MSCR[DSE] is implemented and can be either enabled or disabled.
Anyway, if PTC8 MCSR[DSE = 0], the pad works as GPIO-STANDARD.
Best regards,
Daniel
Hello Heedong Lee,
It cannot be changed.
The N/A option is there for the pads that are GPIO-STANDARD like PTA2.
These pads do not have the MSCR[DSE] implemented.
PTC8 is GPIO-STANDARD-PLUS where MSCR[DSE] is implemented and can be either enabled or disabled.
Anyway, if PTC8 MCSR[DSE = 0], the pad works as GPIO-STANDARD.
Best regards,
Daniel