How accurate is the internal RTC of s32k118

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How accurate is the internal RTC of s32k118

497 Views
feiyiniu
Contributor II

When the customer used the internal RTC timer to test the wake up function, it was found that the timing time was off by 20%.The clock tree output is as follows.Thanks!

 

企业微信截图_1685414901163.png

0 Kudos
2 Replies

484 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@feiyiniu

The precision of the LPO clock is not high, which leads to inaccurate timing of the RTC, but the RTC clock can be compensated through the TCR register to improve the precision of the RTC.

Senlent_0-1685427609664.png

Senlent_1-1685428229218.png

 

This is a document summarized in Chinese, which introduces how to compensate the RTC clock, and hopes to be helpful to your customers.
For users who have strict requirements on the RTC clock, it is recommended to add an external clock circuit

S32K1xx系列MCU应用指南之RTC模块使用详解 

472 Views
feiyiniu
Contributor II

Thank you for your detailed reply

0 Kudos