How I can update BOOT Sequence bit of IVT in S32K3xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How I can update BOOT Sequence bit of IVT in S32K3xx

482件の閲覧回数
Suheel890
Contributor I

I'm trying to use advanced secure boot feature of HSE-B of my S32k314 controller in our project.

after enabling secure boot unable to find any way to update IVT to change BOOT_SEQ from 0 to 1.

because secure boot only impact after BOOT sequence bit is 1.

SBAF will directly release core if BOOT_SEQ bit is 0. if secure boot feature to work HSE should get control.

 

0 件の賞賛
1 返信

465件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Suheel890,

Please use support tickets instead of the public community for HSE related questions, the HSE FW documentation, demos etc. are all under an NDA.

The BCW can be changed here though:

danielmartynek_0-1667823628026.png

 

Regards,

Daniel

 

0 件の賞賛