Hardfault debugging with S32DS_3.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hardfault debugging with S32DS_3.4

ソリューションへジャンプ
762件の閲覧回数
OliverTian
NXP Employee
NXP Employee

Hello,

If you met hardfault when debugging with S32DS 3.4, you can do the follow steps and find the information where triggered the hardfault.

 

  1. Copy the follows data into notepad and save as ‘.gdbinit’


    define armex

      printf "EXEC_RETURN (LR):\n"

      info registers $lr

     

      if (((unsigned int)$lr & 0x4) == 0x4)

      printf "Uses PSP 0x%x return.\n", $psp

      set $armex_base = (unsigned int)$psp

      else

      printf "Uses MSP 0x%x return.\n", $msp

      set $armex_base = (unsigned int)$msp

      end

      printf "xPSR            0x%x\n", *($armex_base+28)

      printf "ReturnAddress   0x%x\n", *($armex_base+24)

      printf "LR (R14)        0x%x\n", *($armex_base+20)

      printf "R12             0x%x\n", *($armex_base+16)

      printf "R3              0x%x\n", *($armex_base+12)

      printf "R2              0x%x\n", *($armex_base+8)

      printf "R1              0x%x\n", *($armex_base+4)

      printf "R0              0x%x\n", *($armex_base)

       

      printf "Return instruction:\n"

      x/i *($armex_base+24)

      printf "LR instruction:\n"

      x/i *($armex_base+20)

    end

     document armex

    ARMv7 Exception entry behavior.

    xPSR, ReturnAddress, LR (R14), R12, R3, R2, R1, and R0

    end

     



  2. Place the file into the folder of S32DS_3.x, like C:\NXP\S32DS_3.4\S32DS\build_tools

  3. In S32DS, S32DS –> Window –> Performances –> Debug –> GDB –> GDB command file
    Set as below
    OliverTian_2-1744856832689.png

     

  4. Debug as general and when meet hardfault, you can input armex in Debugger Console to get more information from stack
    OliverTian_3-1744856832740.png

 

Cheers!

Oliver

 

0 件の賞賛
返信
1 解決策
760件の閲覧回数
OliverTian
NXP Employee
NXP Employee

Hope this will help you.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
761件の閲覧回数
OliverTian
NXP Employee
NXP Employee

Hope this will help you.

0 件の賞賛
返信