HardFault exception in DMA+LPUART+AIPS cooperation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HardFault exception in DMA+LPUART+AIPS cooperation

1,762 Views
SafetyRedneck
Contributor I

Hi All,  I have an issue in AIPS safety reaction of S32K116. We are using LPUART in DMA operation mode. Problem is usage of AIPS.  My expectation is that  HardFault shall ocurre when usage of LPUART is completely disabled by AIPS.  Observed behavior is different.  Processor still works without call HardFault exception.  Only DMA does not work properly.  I am not able to find successful explanation of that.  I can send complete register setting of the processor. I guess, there should be an explanation in processor architecture. For example DMA  like a master is not controlled by AIPS.  MPRA register is not described well in reference manual.  Only three masters are there but nowhere is described what is what. I expect that  0 is core 1 is debugger and 2 is DMA.  But this register is only setting of access into AIPS, not for LPUART periphery. Does somebody knows why HardFault is not called when LPUART is blocked by AIPS and DMA try to write something into its?

0 Kudos
Reply
2 Replies

1,747 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @SafetyRedneck,

Hard_Fault is an exception of the core, it rises when the core detect a bus error, for example.

But if you disable the access of eDMA to a peripheral, for example, LPUART0:

  • MPRA[MTW2] = 0 This master is not trusted for write accesses
  • OPACRJ[TP2] = 1 Accesses from an untrusted master are not allowed

the eDMA should detect an error, e.g  DMA_ES[DBE] (Destination Bus Error, the most-recently recorded error was a bus error on a destination write).

 

Regards,

Daniel

 

0 Kudos
Reply

1,722 Views
SafetyRedneck
Contributor I

Hello DanielMartynek

Thank you for reply.  I can say now where is the problem.  The HardFault interrupt is not caused by AIPS periphery but by Master M0 (core).   AIPS only block access into  specific periphery.  Similar situation is for DMA.  The DMA is master M2. Its reaction is not HardFault interrupt but  DMA Error interrupt. I have solution now.  I have to add DMA error interrupt routine with expected safe reaction. Of course I have to also rework design and SW architecture

Thank you for help.

Best regards