Getting started with S32K144EVB-Q100 + FRDM33771CSPEVB and BATT-14EMU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting started with S32K144EVB-Q100 + FRDM33771CSPEVB and BATT-14EMU

Jump to solution
1,083 Views
davorin_mista
Contributor I

I'm trying to get started with these boards, ultimately looking to play with the BMS code - but I'm still stuck at step1.

Which S32DS version/variant should I use? v1.3 or 2018.R1 or something else?

Which FreeMaster version do I need and where can I find the driver I need?

Where can I find the BMS example source code that's used in the MC3377x EvalGUI? 

Thank you!
Davorin

 

0 Kudos
Reply
1 Solution
1,029 Views
Senlent
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
5 Replies
1,064 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@davorin_mista

I found some information for your reference.

demo code:

https://www.nxp.com/design/analog-expert-software-and-tools/sdk-analog-expert-drivers/14-cell-batter... 

Senlent_0-1671764957305.png

There is a detailed description of the requirements in this download package, the compilation environment requires 2018.R1, FreeMaster should have no version restrictions,

Senlent_2-1671765325899.png

 

 

0 Kudos
Reply
1,060 Views
davorin_mista
Contributor I

Thank you, very helpful. 

I do have 2018.R1 installed however I can't figure out how to get update 11. Here's what I have installed according to About - Installation Details:

davorin_mista_1-1671812605071.png

Also when I import the project I get this warning:

davorin_mista_0-1671812528296.png

Shall I ignore this or do I need to get the Kinetis SDK?

Thanks!
Davorin

0 Kudos
Reply
1,030 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@davorin_mista

I find this SDK download address, you can try to intall it and built again,

https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for... 

 

Senlent_0-1672018633256.png

 

0 Kudos
Reply
1,018 Views
davorin_mista
Contributor I

Thank you, I did install the Update11 as you suggested however when trying to build the Monitoring project I get compilation errors:

davorin_mista_1-1672254952318.png

 

Also, not sure if it matters but after importing the project I first get a warning about the Kinetis version:

davorin_mista_0-1672254857321.png

I chose "Yes" then the project finished importing without errors/warnings.

0 Kudos
Reply
1,016 Views
davorin_mista
Contributor I

Sorry, I was able to overcome this by starting from scratch, i.e. re-extracting the EMBEDDED-SW-BCC-MC33771C ZIP file - seems all good now!

0 Kudos
Reply