Getting started with FreeRTOS in S32K DS 3.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting started with FreeRTOS in S32K DS 3.5

ソリューションへジャンプ
3,066件の閲覧回数
JaGaISS
Contributor I

Hi All,  New to the S32K DS and am trying to get some code working with FreeRTOS for the K344.

I am working off SW32K3_FreeRTOS_10.6.0_4.0.0_CD_D2312_ReleaseNotes. From these:

Installation flow:
1. Install S32Design Studio 3.5: S32DS.3.5_b220726_win32.x86_64.exe
2. Install Update 8 for S32DS: com.nxp.s32ds.update_3.5.8.20231116041033.zip
3. Install development package for S32K3XX: com.nxp.s32ds.s32k3xx.update_3.5.8.20231116045533.zip
4. Install development package for S32K396: SW32K39x_S32DS_3.5.6_D2309.zip
5. Install RTD updatesite: SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip

 

For steps 2, 3 and 4; where do I find these zip files. They do not appear to be included with the standalone "SW32K3_FreeRTOS_10.6.0_4.0.0_CD_D2312" package that I started with. I searched the forums for a while, but couldn't seem to find them.

In general what is the best way to find these update packages (there are so many).

I tried skipping ahead to just:

"Open Help -> S32DS Extensions and Updates. From the next windows,
select "FreeRTOS for S32K3XX_S32M27x" then click Install/Update"

But unsurprisingly, this fails due to a missing dependency. 

Any help is appreciated. Thanks.

0 件の賞賛
返信
1 解決策
3,026件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @JaGaISS 

I am attaching the links where you can download the corresponding packages. 

2 > S32 Design Studio 3.5 Update 8 D2311

3 and 4 > S32K3 Standard Software > Automotive SW - S32K3 - S32 Design Studio >  S32 Design Studio 3.5.6 RTM with support for S32K39x devices and S32 Design Studio 3.5.8 Development Package with support for S32K3xx devices. 

The zip file you will download from those links should be added to S32DS through S32DS Extensions and Updates > Add Update Sites.

 

B.R.

VaneB

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,027件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @JaGaISS 

I am attaching the links where you can download the corresponding packages. 

2 > S32 Design Studio 3.5 Update 8 D2311

3 and 4 > S32K3 Standard Software > Automotive SW - S32K3 - S32 Design Studio >  S32 Design Studio 3.5.6 RTM with support for S32K39x devices and S32 Design Studio 3.5.8 Development Package with support for S32K3xx devices. 

The zip file you will download from those links should be added to S32DS through S32DS Extensions and Updates > Add Update Sites.

 

B.R.

VaneB

0 件の賞賛
返信