Gerber files for Motor Kit board 29379_B2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gerber files for Motor Kit board 29379_B2

ソリューションへジャンプ
1,154件の閲覧回数
Georgio_69
Contributor II

Hello,

We are trying to design a new shield for the S32K144 evaluation board. Is it possible to have all the electronic files (Schematic, BOM, gerber files) for the board DEVKIT-MOTORGD (pdf file SPF-29379_B2)?

It will be very helpful for several reasons especially to have the connectors at the same place. Gerber files is the most important point.

Thanks a lot

Kind regards,

Georges FRAPPA

0 件の賞賛
返信
1 解決策
1,112件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

The schematic is created in ORCAD. 
The layout file is created in Cadence Allegro.

元の投稿で解決策を見る

3 返答(返信)
1,143件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Georges FRAPPA,

From DEVKIT-MOTORGD: Low-Cost Motor Control Solution for DEVKIT Platform, you can download the DEVKIT-MOTORGD BOM Files and DEVKIT-MOTORGD Layout Files and DEVKIT-MOTORGD Schematics

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,127件の閲覧回数
Georgio_69
Contributor II
Hello, Thanks very much for all these files. It seems that schematic was done with ORCAD Capture, is it right? What about the layout? done also with ORCAD? or with other SW like Eagle for example? Thanks for the confirmation Best regards, Georges
0 件の賞賛
返信
1,113件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

The schematic is created in ORCAD. 
The layout file is created in Cadence Allegro.