Generate Different frequencies with Single FTM-PWM channel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Generate Different frequencies with Single FTM-PWM channel

866件の閲覧回数
Learner
Contributor III

Hi NXP Team

I am using S32k118 in my project, and as per my project requirement, I have to generate two different frequencies i.e. 50khz and 625Hz.
In S32118 only two FTM channels are available i.e. FTM0 and FTM1

FTM1 is used as Flextimer Modulus Counter and FTM0 is used as PWM generator.
Is it possible to generate both 50khz and 625hz PWM from FTM0?
Please suggest 
thanks 

 

タグ(2)
0 件の賞賛
返信
1 返信

851件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Learner

      It's not possible to generate different PWM frequencies under the same module base,

BR!

     Jim,