GPIO noise issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO noise issue

1,562 Views
Bhuvana
Contributor I

MCU:FS32K144UAT0VLLT
100LQFP

How to remove noise in the GPIO input pins and how to use digital filter and passive filter what it will do exactly? I have enabled digital filter and system clock is FIRC.

0 Kudos
Reply
1 Reply

1,543 Views
JRoberto
NXP TechSupport
NXP TechSupport

Hello @Bhuvana 

That depends on your signal conditions and the source of the noise.

The passive filter is just an internal resistor but it's not always available. Refer to the device data sheet for filter characteristics. You will found a table that indicates if the Passive filter is enabled.

JRoberto_0-1661511016409.png

The Digital filter will introduce delay in your signal. So in case the noise you mention is generated by a push button (That creates a bounce in the signal). Then digital filtering might be able to help you.

You can refer to the thread linked bellow to see some configuration details.

Solved: Re: using digital filter on external interrupt pin... - NXP Community

Best regards

0 Kudos
Reply