Freerunning Counter (FTM, S32K1) using RTD 1.0.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freerunning Counter (FTM, S32K1) using RTD 1.0.1

Jump to solution
782 Views
superbird
Contributor I

Hello,

I want to implement a simple 16-bit freerunning counter using RealTime Drivers (RTD) but I cannot find the proper functions here. In the SDK there are the functions FTM_DRV_InitCounter, FTM_DRV_CounterStart, FTM_DRV_CounterStop, FTM_DRV_CounterRead, ... but I cannot find equivalent functions in the RTD set. Additionally I need a function to reset the counter value like provided by FTM_DRV_SetCounter in the SDK.

Any help/example is greatly appreciated. 

Best Regards,

 

 

 

0 Kudos
Reply
1 Solution
746 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@superbird

The functions that can be realized by these SDKs are exactly the same.

I don't know how you used the FTM module to achieve the function in the old version, but it is sure that the RTD driver can also be implemented,

I checked the "Ftm_Gpt_Ip.c" file, which is the same as the "ftm_mc_driver.c" provided by RTM almost the same function

View solution in original post

0 Kudos
Reply
3 Replies
761 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@superbird

please take a look at the demo "Ftm_Gpt_Example_S32K144" in S32 DS

I attached the example description for you know.

1. Example Description
The application includes a Design Studio project, that uses predefined configurations for the IP layer only (Port_Ci, Clock, IntCtrl, Ftm and Osif).

The application uses the IP layer functionality to trigger a timer interrupt. Notification function increase a count variable by 1 and toggle state pin LED on board.
1.1 The application software functionality
- Clock_Ip_Init
     Initializes the clock
- Port_Ci_Port_Ip_Init
     Initializes the pins used by the application using the Port_Ci API.
- IntCtrl_Ip_EnableIrq & IntCtrl_Ip_InstallHandler
     Enable the interrupt used by the application and set the correct handler for it.
- Ftm_Gpt_Ip_Init, Ftm_Gpt_Ip_InitChannel, Ftm_Gpt_Ip_EnableChannelInterrupt & Ftm_Gpt_Ip_StartTimer
     Initialize the Ftm IP layer, to start the selected timer and to enable its notification that will be used for periodically blinking an LED
- Runs the while(1) loop and, based on the Ftm notification, uses the Gpio_Dio_Ip_TogglePins of the Gpio_Dio IP API to toggle the pin connected to the LED

 

0 Kudos
Reply
752 Views
superbird
Contributor I

Hi@Senlent,


I know this example but unfortunately I don't think that this example fits for me.

I want to generate a time base (microseconds, freerunning). So generating an interrupt (every microsecond) is not an option for me. I wonder because the the counter functionality was included in the previous SDK.

 

0 Kudos
Reply
747 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@superbird

The functions that can be realized by these SDKs are exactly the same.

I don't know how you used the FTM module to achieve the function in the old version, but it is sure that the RTD driver can also be implemented,

I checked the "Ftm_Gpt_Ip.c" file, which is the same as the "ftm_mc_driver.c" provided by RTM almost the same function

0 Kudos
Reply