FreeRTOS 10 for S32K144

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FreeRTOS 10 for S32K144

1,139 次查看
sdrb
Contributor II

Hello,

I'd like to write some simple testing application for S32K144 using FreeRTOS 10. I am using S32DS 2018.R1 under Linux. Unfortunately there is something wrong with S32DS under Linux and I cannot select anywhere FreeRTOS in S32DS. I've seen a few tutorials on the net where FreeRTOS can be used from S32DS but I have no such option in my version.

Thus I'm planning to create FreeRTOS project manually. I guess I need dedicated FreeRTOS for S32K144 so I'd like to ask if there are official FreeRTOS v10 sources for S32K144 published somewhere? 

标记 (1)
0 项奖励
1 回复

773 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Witold Kowolik

The SDK is not supported in Linux environment, sorry for the inconveniences that this might cause you.

S32DS and S32K1XX SDK on Linux 

Regards

0 项奖励