For new development cycle which version of packages is suggestable by NXP for S32K144 non autosar

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

For new development cycle which version of packages is suggestable by NXP for S32K144 non autosar

1,110 次查看
SivaB
Contributor III

suggest the correct SDK, GCC tool chain & RTD version for S32K144 to use LIN communication.

1) S32DS 3.4 / 3.5 

2) RTD SW32K1_RTD_4_4_1_0_1_D2202 / S32SDK_S32K1XX_RTM_4.0.3

3) LIN Stack 1.0.1 / 1.0.2

4) DRV driver / IP driver

0 项奖励
回复
1 回复

1,102 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@SivaB

Users can understand some differences between RTD and RTM versions from this answer

https://community.nxp.com/t5/S32K/difference-between-s32k1-sdk-and-s32k1-rtd/m-p/1637711#M22289 

For applications developed by non-autosar, I personally prefer to use the RTM version, because the RTM SDK will be more concise. If you use the RTM SDK version, you can only use S32 DS V3.4, GCC V6.3.1

Use RTD to develop Non-Autosar applications, you can try to use the latest S32 DS V3.5, please use the same LIN Stack as the RTD version

0 项奖励
回复