Flashing a MBDT example model in to MR-CANHUBK3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashing a MBDT example model in to MR-CANHUBK3

1,246件の閲覧回数
HariRam_111
Contributor II

Hello!

I am just getting started with MR-CANHUBK3

I am trying to flash the Target board with CAN examples from the MBDT toolbox.

But I get the following error.

HariRam_111_0-1697006322372.png

I see that the MR-CANHUBK3 has no traditional openSDA port available.

How do I proceed with downloading the example on to the board if openSDA port is not available on the board?

Thanks for the help

 

 

0 件の賞賛
返信
3 返答(返信)

1,220件の閲覧回数
HariRam_111
Contributor II

Can I use S32 Debug Probe as the external debugger probe? (I already tried this though, I am getting the same error message I posted above when I was trying to flash)

Or should I use something like Segger J-Link EDU Mini- JTAG/SWD Debugger?
Thanks again for the help!

 
0 件の賞賛
返信

1,200件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@HariRam_111

S32 Debug Probe

Senlent_0-1697076602900.png

From the picture above, you can see the S32K is not in the support list.

Here I recommend using Lauterbach, Pemicro Multilink, Segger-J-link.

 

"Segger J-Link EDU Mini- JTAG/SWD Debugger"

You need to check with Segger technical support as this is not a commonly used debugger

 

0 件の賞賛
返信

1,227件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@HariRam_111

You need an external debugger

Senlent_0-1697011458463.png

 

0 件の賞賛
返信