Failed to run generator "eMcem_TS_T40D2M8I0R0_GeneratorId" (mode: "generate") for module "eMcem_TS_T

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to run generator "eMcem_TS_T40D2M8I0R0_GeneratorId" (mode: "generate") for module "eMcem_TS_T

473 Views
AElnemr
Contributor I

Hello,
I'm trying to generate eMcem module through DaVinci CFG using external generator. the error logs as the following:-

Copyright 2003-2020 Elektrobit Automotive GmbH
INFO 23-08-29,14:43:49 (12145) Using a shortened feature name ("EB_TS_MOD_USeMcem_TS_T40D2M8I0" instead of "EB_TS_MOD_USeMcem_TS_T40D2M8I0R0") for license check.
INFO 23-08-29,14:43:49 (12145) Using a shortened feature name ("EB_TS_MOD_USeMcem_TS_T40D2M8I0" instead of "EB_TS_MOD_USeMcem_TS_T40D2M8I0R0") for license check.
INFO 23-08-29,14:43:49 (12145) Using a shortened feature name ("EB_TS_MOD_USeMcem_TS_T40D2M8I0" instead of "EB_TS_MOD_USeMcem_TS_T40D2M8I0R0") for license check.
INFO 23-08-29,14:43:49 (2202) Reading file "C:\Users\aelnemr\Desktop\proj5674_master_dev_hvch_pipp_Copy\Config\ECUC\Tresos_Mcal_Arxml\HVCH_eMcem_ecuc_tresos.arxml"
WARNING 23-08-29,14:43:49 (1055) Removed node "IMPLEMENTATION_CONFIG_VARIANT": The schema does not define a parameter with name "IMPLEMENTATION_CONFIG_VARIANT" in container "/TS_T40D2M8I0R0/eMcem".
WARNING 23-08-29,14:43:49 (1055) Removed node "POST_BUILD_VARIANT_USED": The schema does not define a parameter with name "POST_BUILD_VARIANT_USED" in container "/TS_T40D2M8I0R0/eMcem".
INFO 23-08-29,14:43:49 (2164) Verify module configuration "/eMcem/eMcem"
INFO 23-08-29,14:43:49 (13030) Running generator "eMcem_TS_T40D2M8I0R0" in mode "generate" for module "eMcem_TS_T40D2M8I0R0"
INFO 23-08-29,14:43:49 (20053) Generating file C:\Users\aelnemr\Desktop\proj5674_master_dev_hvch_pipp_Copy\Appl\GenData\output\eMcem.epc
INFO 23-08-29,14:43:49 (13030) Running generator "eMcem_TS_T40D2M8I0R0_GeneratorId" in mode "generate" for module "eMcem_TS_T40D2M8I0R0"
ERROR 23-08-29,14:43:49 (2191) Failed to run generator "eMcem_TS_T40D2M8I0R0_GeneratorId" (mode: "generate") for module "eMcem_TS_T40D2M8I0R0"
ERROR 23-08-29,14:43:49 (1806) Parsing file "C:\Users\aelnemr\Desktop\Valeo_std_R30_S32K14x_Iar_1.0.0\ThirdParty\Mcal_S32k\Supply\tresos27_\plugins\eMcem_TS_T40D2M8I0R0/generate_PC/src/eMcem_Cfg.c (signed)", line "114"
The XPath-expression "ecu:get('eMcem.eMcemCortexM4')='true'" caused an error: (35016) Cannot get a resource file for target ARM and derivate S32K14X. Maybe this is due to module restrictions.
ERROR 23-08-29,14:43:49 (2170) Failed to generate file "C:\Users\aelnemr\Desktop\Valeo_std_R30_S32K14x_Iar_1.0.0\ThirdParty\Mcal_S32k\Supply\tresos27_\plugins\eMcem_TS_T40D2M8I0R0/generate_PC/src/eMcem_Cfg.c (signed)"
ERROR 23-08-29,14:43:49 (1806) Parsing file "C:\Users\aelnemr\Desktop\Valeo_std_R30_S32K14x_Iar_1.0.0\ThirdParty\Mcal_S32k\Supply\tresos27_\plugins\eMcem_TS_T40D2M8I0R0/generate_PC/include/eMcem_Cfg.h (signed)", line "103"
The XPath-expression "ecu:get('eMcem.eMcemCortexM0')='true'" caused an error: (35016) Cannot get a resource file for target ARM and derivate S32K14X. Maybe this is due to module restrictions.
ERROR 23-08-29,14:43:49 (2170) Failed to generate file "C:\Users\aelnemr\Desktop\Valeo_std_R30_S32K14x_Iar_1.0.0\ThirdParty\Mcal_S32k\Supply\tresos27_\plugins\eMcem_TS_T40D2M8I0R0/generate_PC/include/eMcem_Cfg.h (signed)"

aslo, I checked my Java version as it was taken in considiration in many other solutions looks like mine and it as the following:-

java version "1.8.0_202"
Java(TM) SE Runtime Environment (build 1.8.0_202-b08)
Java HotSpot(TM) 64-Bit Server VM (build 25.202-b08, mixed mode)

So, please if anyone faced the same problem give me solution.
Thanks.

0 Kudos
Reply
0 Replies