Facing Issue with Make file S32K144 [crt0.o : No such Directory]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Facing Issue with Make file S32K144 [crt0.o : No such Directory]

1,550 次查看
AbhishekK
Contributor II

Hello Helpers ,
I am facing below issue with Make file .I know the issues is it unable to link the library files [newlib] .I am not able to find solution .Please help me with this.

Screenshot 2023-05-01 023754.png

 

标记 (3)
0 项奖励
回复
4 回复数

1,313 次查看
AbhishekK
Contributor II

Hi Akhileshverneka

to resolve issue 

go to compiler location C:\NXP\gcc-6.3-arm32-eabi\arm-none-eabi\newlib it contains lib folder .

copy that lib folder and paste it to C:\NXP\gcc-6.3-arm32-eabi\arm-none-eabi\ location 

problem will be resolved 

0 项奖励
回复

1,325 次查看
akhileshverneka
Contributor II

Hi All,

I am also facing the same issue.

Please anyone could post the solution to solve this issue.

Thank you in advance

0 项奖励
回复

1,526 次查看
mikedoidge
NXP Employee
NXP Employee

Additional notes from @AbhishekK :

I facing Below error .Please help me with it 

d:/nxp/s32ds.3.4/s32ds/build_tools/gcc_v6.3/gcc-6.3-arm32-eabi/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/real-ld.exe: cannot find crt0.o: No such file or directory

what should  I do?

.I am using S32K144 MCU .and I am using GNU compiler for it .

this is demo Project from Electrobit .I have downloaded from electrobit site . EBtresos Evaluation edition .I am using make files to compile the project not any IDE  . Compiler is GNU .I am not able to upload any data from here 

I am not able to add newlib library in my project .I have added in sysroot path this library path but still it is taking below path

c:/nxp/s32ds_arm_v2.2/s32ds/build_tools/gcc_v4.9/gcc-arm-none-eabi-4_9/bin/../lib/gcc/arm-none-eabi/4.9.3/../../../../arm-none-eabi/bin/ld.exe: cannot find -lc
collect2.exe: error: ld returned 1 exit status

0 项奖励
回复

1,462 次查看
cuongnguyenphu
NXP Employee
NXP Employee

What is GCC version you're using? Seems that this project need version 6.3 why you're installing GCC version 4.9.
Let's ask Elektrobit again for the version compiler of this demo sample

0 项奖励
回复