FTM1 IRQ number on S32K144 Microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FTM1 IRQ number on S32K144 Microcontroller

Jump to solution
418 Views
mr_jeffs
Contributor II

Hallo 

I am working with S32K144 microcontroller. I would like to measure a clock signal and for that I would like to use the input capture mode of FTM1 timer module. But to enable the FTM1 interrupt using the NVIC engine, I do not know the FTM1_IRQ number. I got actualy two questions:

1. Can someone tell me the FTM1_IRQ number?

2. Is there any document or table which shows the IRQ numbers of different modules?. If so, could you please tell me where/how can I find that 

Thank you

Regards

0 Kudos
Reply
1 Solution
410 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@mr_jeffs

I copied this informations as shown below

Senlent_0-1667785577435.png

 

this file can be found in S32K-RM attachment and the file name is S32K1xx_DMA_Interrupt_mapping.xlsx.

 

BR!

 

View solution in original post

1 Reply
411 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@mr_jeffs

I copied this informations as shown below

Senlent_0-1667785577435.png

 

this file can be found in S32K-RM attachment and the file name is S32K1xx_DMA_Interrupt_mapping.xlsx.

 

BR!