Hi to everyone,
I'm working with S32K32118 EVB and S32DS.3.5
Through S32 configuration tool, I've created a PWM waveform on FTM0, CH0.
I wonder if is possible to get an interrupt/callback for every rising or falling edge of the PWM (or at least when a new period is starting/ended) without adding/using FTM1 module and other channels.
Thanks, Federico
Hi @Fede
Every FTM channels have an interrupt that you can enable whit the register Channel(n) Status And Control (C0SC - C7SC) bit 6(CHIE). So it is not necessary to configure another FTM.
I suggest you take a look at section 47.5.4(Channel Modes) onwards of the reference manual and the application note: Features and Operation Modes of FlexTimer Module on S32K.
B.R.
VaneB
Hi VaneB,
thank you for your support. My mistake: I wasn't deleting correctly the Interrup flag inside the interrupt handle routine. Now I can see the correct behaviour of the Interrupt.
Regards, Federico
Hi @Fede
Thanks for the feedback, if you have any problem let me know.