Hi There,
In Our application is present an FS26 for off-chip safety.
The application is divided in Bootloader and application code .
The FS26 watchdog is programmed by application to 120ms, but this is too small for bootloader.(downloading code) : we need to program watchdog ad least 300ms (or more for further applications).
Is it possible to program FS26 with a W1 whatchdog value for the bootload (downloading code) and a smaller W2 value at the start of application (without resetting s32k344?)
If it is possible, how to use FS26RTD3.0.0 Drivers for this purpose ?
Best Regards
Fabio
解決済! 解決策の投稿を見る。
Hi
On the fly to change the WD, you have to change it by below WDW_PERIOD[3:0]bits in the FS_WDW_DURATION register, you can try it.
The duration of the watchdog window is configurable from 1.0 ms to 1024 ms with the WDW_PERIOD[3:0] SPI bits.
The new watchdog window is effective after the next watchdog refresh.
Hi
I mean if it is possible to change FS26 Whatchdog value "On the Fly".
For example WD = 512ms (Bootloader run) then then switch to WD = 120ms (when switch to application).
This should be happen without the need of resettting s32k344 (SW FUNC reset or others).
If it is possible, I would know how to deploy it by using FS26 RDT 3.0.0 (sw functions needed, scheduling points...)
Best Regards
Fabio
Hi
On the fly to change the WD, you have to change it by below WDW_PERIOD[3:0]bits in the FS_WDW_DURATION register, you can try it.
The duration of the watchdog window is configurable from 1.0 ms to 1024 ms with the WDW_PERIOD[3:0] SPI bits.
The new watchdog window is effective after the next watchdog refresh.
Hi
Here I only support FS26 and don't know too much about bootloader.
Do you mean to change the WD duration into longer time as below showed?