FS26 Wake1 pin is shorted supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 Wake1 pin is shorted supply

264 Views
mogilipuri_harish
Contributor II

hello team,

 

we are using FS26 SBC in our design. 

1. what will happen if wake pin shorted to 5V or 12V supply??

2. what will happen if wake pin makes continuously high??(we set wake pin polarity as 1 detected wake signal activated)

0 Kudos
3 Replies

207 Views
mogilipuri_harish
Contributor II

hi,

thanks for quick replay....

1.how we will know whether FS26 is in DFS and standby mode?

2. what are pins are active when DFS and standby mode? 

3. is it possible to get the status from GPIO weather SBC in DFS state or standby mode?

4. what will happened when wake 1 & 2 pins are shorted GND?

5. for wakeup the SBC we need to connect wake 1 & 2 pins or either 1 pin is ok?

0 Kudos

180 Views
guoweisun
NXP TechSupport
NXP TechSupport
  1. how we will know whether FS26 is in DFS and standby mode?

[gw]Different regulators status with different modes.

guoweisun_0-1694671425126.png

 

guoweisun_1-1694671425215.png

 

  1. what are pins are active when DFS and standby mode? 

[gw]above answer1.

  1. is it possible to get the status from GPIO weather SBC in DFS state or standby mode?

[gw]No

4:what will happened when wake 1 & 2 pins are shorted GND?

[gw]wake up function depends on the setting below:

guoweisun_2-1694671425306.png

 

  1. for wakeup the SBC we need to connect wake 1 & 2 pins or either 1 pin is ok?

[gw]Please see wake conditions:

guoweisun_3-1694671425321.png

 

0 Kudos

225 Views
guoweisun
NXP TechSupport
NXP TechSupport

From this below internal diagram of WAKE pins, I think no problem for short to 5V or 12V but should more current consumption.

guoweisun_0-1694567230382.png

 

0 Kudos