Example_S32K144_RTC_VLPS_S32DS_ARM_22_v2 can not enter into VLPS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example_S32K144_RTC_VLPS_S32DS_ARM_22_v2 can not enter into VLPS?

1,311件の閲覧回数
Ada_Lovelace
Contributor IV

Hi,all

I use the demo:Example_S32K144_RTC_VLPS_S32DS_ARM_22_v2, it is used to test VLPS function,but when I debug it, it will not enter the VLPS mode, I check the SMC_PMSTAT,it is still in RUN mode.

Ada_Lovelace_0-1718953424445.png

Ada_Lovelace_1-1718953490796.png

Then I debug the project, SMC_PMCTRL can not change, it is not in VLPS. I put led in board, exit the debug, restart the board,it still no work.

Ada_Lovelace_2-1718953573508.png

I use the S32K144 EVB-Q100 board, can someone tell me how to enter the VLPS mode?

 

 

 

0 件の賞賛
返信
1 返信

1,290件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Ada_Lovelace 

We provide Power Management application note including demo projects which explains all the steps in detail. It can be downloaded from S32K1 Microcontrollers for Automotive General Purpose. 

The application note can be found here AN5425: Power Management for S32K1xx – Application Note. 

The associated demo projects can be downloaded here AN5425SW – Application note software for AN5425. 

 

B.R.

VaneB

0 件の賞賛
返信