Eval board as debugger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Eval board as debugger

跳至解决方案
6,842 次查看
arkadyosh
Contributor III

Hi,
I have FRDMPK144-Q100 eval board and I want to use it as debugger for my custom board with S32K144 uC. Target board use SWD as debug/program interface. How to connect eval board with custom board? Some changes in eval board are necessary?

I use S32 Design Studio for ARM.

Regards

标记 (5)
1 解答
6,071 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can use J14 pinheader. I connected together two FRDMPK144-Q100 boards by J14 connectors and I'm able flash/debug them together. 

If you like to flash only your custom target - you will need to remove connections (at least some of them) between J14 and FRDMPK144-Q100 MCU. I tried flash the second EVB without power on first S32K144 - but it doesn't work - the second EVB is held in reset. 

Jiri 

在原帖中查看解决方案

0 项奖励
回复
9 回复数
6,071 次查看
arkadyosh
Contributor III

Hi,

Thanks Jiri, I can now flash my custom board. Just remove connections between J14 SWD_DIO, SWD_CLK pins and target eval board uC and change bootloader in OpenSDA to Segger OpenSDA V1(SEGGER - The Embedded Experts - Downloads - J-Link / J-Trace ).

Regards,

Arkadiusz

6,071 次查看
yuganshbansal
Contributor I

Hello,

I am using S32K144EVB as an OPENSDA debugger to debug my custom FS32K144UAVLLT micro-controller. I have also cut the SWD_DIO and SWD_CLK from the J1-06. When bootloader is with original OPENSDA firmware, i am able to debug the custom uC but i am getting "Target MCU Mismatch" error. When bootloader is changed with Segger OPENSDA V1(j link), then also i am able to debug the custom uC, but i am not able to run my example Toggle_LED program.

Can you think of a possible reason ? Was your program working fine when you debug your custom uC ? 

0 项奖励
回复
6,071 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

well, I don't know in detail your design, but what can sure work is remove all connections from JTAG pinheader  to EVB MCU. Otherwise - you need to experiment. Also don't forget connect grounds on your custom board and OpenSDA. 

Jiri

0 项奖励
回复
6,071 次查看
yuganshbansal
Contributor I

Hi, 

I am sharing my programming interface with you. Please advise on the same.

pastedImage_1.png

0 项奖励
回复
6,071 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

you also need add Reset signal from J12 (JTAG). Anyway - are you sure that the crystal is working okay on breadboard? The crystal should be close as possible to MCU. 

Jiri

0 项奖励
回复
6,071 次查看
sparkee
Contributor V

jirikral

Can you explain your response claiming reset is needed?

0 项奖励
回复
6,071 次查看
sparkee
Contributor V

I know this is an old thread but I can't find where the SDA_RST pin goes to the MCU on the EVB schematic.  It goes to the barRESET pin on the K20.  Am I wrong that the reset isn't necessary for programming an external MCU?

I would like to use a 6 pin header for programming my board.  Tag Connect shows a specific cable with JTAG pinout that has RESET on there but not JTAG_TDO.  If I'm wanting to program and debug using the S32K144EVB as my programmer, can I use the proposed pinout from Tag Connect or should I move to a 10pin programming header?

pastedImage_1.png

0 项奖励
回复
6,072 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can use J14 pinheader. I connected together two FRDMPK144-Q100 boards by J14 connectors and I'm able flash/debug them together. 

If you like to flash only your custom target - you will need to remove connections (at least some of them) between J14 and FRDMPK144-Q100 MCU. I tried flash the second EVB without power on first S32K144 - but it doesn't work - the second EVB is held in reset. 

Jiri 

0 项奖励
回复
4,560 次查看
Dileep1441
Contributor I

Hi,

I'm trying to Flash the Custom Board(S32K144) with Evaluation Board (FRDM board S32K144) over the J14 Connector.

Could you please share the Pin to Pin Connection Details at J14 Connector and Hardware Changes(if any) also Programming Process for Custom Board.

 

Thanks in Advance.

0 项奖励
回复