Ethernet (board: S32K3X4EVB-T172) _transceiver TJA1103

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet (board: S32K3X4EVB-T172) _transceiver TJA1103

3,764 Views
imlaam
Contributor II

Dear Expert,

We bought S32K3X4EVB-T172 Evaluation Board for development. (S32K3X4EVB-T172 Evaluation Board for Automotive General Purpose | NXP Semiconductors)

We are currently having problems initializing the TJA1103 transceiver. We have downloaded and installed the TCPIP stack (refer: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D ) and the source code includes the Init for the TJA1103 transceiver.
But when we tried it, the code didn't work. And here is the image for the core when we debug.

imlaam_0-1693900939208.pngimlaam_1-1693900951880.png

Could you please help us to feedback about these cases?

Thanks,
Lam Phan

Tags (3)
4 Replies

3,595 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

which kind of tcpip version do you use? A tcpip stack 1.0.3 supports T172 board as per its release note

PetrS_0-1694001114085.png

BR, Petr

0 Kudos
Reply

3,520 Views
imlaam
Contributor II

Hi,

I have addition question: Can we use MII interface for board S32K3X4EVB-T172 REV B

If yes, please tell me the method to configure a board to MII mode.

BR,

Lam Phan

0 Kudos
Reply

3,423 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

S32K3X4EVB-T172 Hardware User Manual discussed configuration of enet interface (MII vs RMII) between board revisions in chapter 11.
Attached is short guide for LWIP example porting.

Hope it helps.

BR, Petr

0 Kudos
Reply

3,548 Views
imlaam
Contributor II

HI,

I currently use tcpip version 1.0.3 and board S32K3X4EVB-T172 REV B

BR, Lam Phan

0 Kudos
Reply