Ethernet (board: S32K3X4EVB-T172) _transceiver TJA1103

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet (board: S32K3X4EVB-T172) _transceiver TJA1103

3,900 次查看
imlaam
Contributor II

Dear Expert,

We bought S32K3X4EVB-T172 Evaluation Board for development. (S32K3X4EVB-T172 Evaluation Board for Automotive General Purpose | NXP Semiconductors)

We are currently having problems initializing the TJA1103 transceiver. We have downloaded and installed the TCPIP stack (refer: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D ) and the source code includes the Init for the TJA1103 transceiver.
But when we tried it, the code didn't work. And here is the image for the core when we debug.

imlaam_0-1693900939208.pngimlaam_1-1693900951880.png

Could you please help us to feedback about these cases?

Thanks,
Lam Phan

标记 (3)
4 回复数

3,731 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

which kind of tcpip version do you use? A tcpip stack 1.0.3 supports T172 board as per its release note

PetrS_0-1694001114085.png

BR, Petr

0 项奖励
回复

3,656 次查看
imlaam
Contributor II

Hi,

I have addition question: Can we use MII interface for board S32K3X4EVB-T172 REV B

If yes, please tell me the method to configure a board to MII mode.

BR,

Lam Phan

0 项奖励
回复

3,559 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

S32K3X4EVB-T172 Hardware User Manual discussed configuration of enet interface (MII vs RMII) between board revisions in chapter 11.
Attached is short guide for LWIP example porting.

Hope it helps.

BR, Petr

0 项奖励
回复

3,684 次查看
imlaam
Contributor II

HI,

I currently use tcpip version 1.0.3 and board S32K3X4EVB-T172 REV B

BR, Lam Phan

0 项奖励
回复