Error when using S32K14 AutoSAR OS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error when using S32K14 AutoSAR OS

7,458 次查看
geweilin
Contributor II

I installed tresos Studio 23.0 , Autosar OS(SW32K14-OS401-RTM-1.0.0 b4.0.98)  and Autosar MCAL(SW32K14-MCAL401-RTMC-1.0.4).

The result is that MCAL is used and tested good.

But when I try to generate OS configuration file(.c,.h), it gives the following 3 error:

1. Failed to run generator "Os_TS_T40D2M4I0R98GeneratorId" (mode: "generate") for module "Os_TS_T40D2M4I0R98"

2. Error in external generator: fatal 0201: 'S32K' target is not supported by your license!
Used generator commandline: C:\EB\tresos23\..\..\NXP\AUTOSAR\S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0\os_ts\eclipse\plugins\Os_TS_T40D2M4I0R98\..\..\..\..\ssc\bin\generator\sg.exe C:\Users\weilin.ge\Desktop\os_sample_sc1\output\generated\epc\project.epc

3. The external generator for module Os_TS_T40D2M4I0R98 terminated with exit code 9
Used generator commandline: C:\EB\tresos23\..\..\NXP\AUTOSAR\S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0\os_ts\eclipse\plugins\Os_TS_T40D2M4I0R98\..\..\..\..\ssc\bin\generator\sg.exe C:\Users\weilin.ge\Desktop\os_sample_sc1\output\generated\epc\project.epc

I want to what's the problem reason? and how to resolve it? 

Thanks.

标记 (3)
12 回复数

7,033 次查看
allenlw
Contributor III

the OS generator need a java run enrivonment, so you need to download a JRE from the official site and install it . I think it wil solve your problem.

7,034 次查看
qianyanhua
Contributor I

When I use the sample,it's OK;but when I create my project,or change the sample,it's the same error "The external generator for module Os_T40D2M4I0R98 terminated with exit code 7".

0 项奖励
回复

7,034 次查看
allenlw
Contributor III

do you install the JRE like I said before?

0 项奖励
回复

7,034 次查看
qianyanhua
Contributor I

Yes,I did it,but when I create a new project ,the error reappears.

0 项奖励
回复

7,034 次查看
allenlw
Contributor III

I don't know what exactly the problem you meet, but you can find a decimal number at the front end of the error message, then look it up at the 21.4 list of messages in the AUTOSAR_OSS32K_TR, it's a document in the OS installation folder, hope this will help you.

0 项奖励
回复

7,034 次查看
qianyanhua
Contributor I

Yes,before I install JRE, the sample generate is not OK,but after that,it's OK.Error reappears when I use a new project,or change the samle.

qianyanhua@cncaea.cn

0 项奖励
回复

7,034 次查看
xinxin_you
Contributor II

I meet this problem.How to slove it?

0 项奖励
回复

7,034 次查看
江洪秦
Contributor I

I  have the same problem. Do you know how to solve it ?

0 项奖励
回复

7,032 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

I created ticket with your question for Automotive Software team. The will contact you back directly via email. Please let me know here, if you do not receive reply until end of this week.

Regards,

Martin

0 项奖励
回复

6,374 次查看
Simin
Contributor II

Hi,

        I also have this problem too,and don't know how to solve it,pls support me,thank you very much

Best regards,

simin

0 项奖励
回复

6,748 次查看
lubo_NEW
Contributor III

I meet this problem.How to slove it?

0 项奖励
回复

7,032 次查看
江洪秦
Contributor I

Hi, Martin,

 Could you share the solved method?

0 项奖励
回复