Error "make***[hello.elf] Error 1"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error "make***[hello.elf] Error 1"

3,094件の閲覧回数
ie703092
Contributor I

Good day, we have a problem that by joining FreeRtos along with other functionality such as Flextimer or I2C, we generate that error. Reading in some forums say that some are by the linker and others because the memory was consumed. The error that appears in the legend is the following "make *** [hello.elf] Error" We are using S32 studio for the evaluation board s32k144.#error #linker #s32studio

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,787件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share output from build console? 

Jiri

0 件の賞賛
返信

2,787件の閲覧回数
ie703092
Contributor I

0 件の賞賛
返信

2,787件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

actually - I mean build console - the very first tab. There should be some description related to error (for example missing header...). 

Jiri

0 件の賞賛
返信