Error of example [iseled_freemaster_s32k144]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error of example [iseled_freemaster_s32k144]

193 Views
alstlr926
Contributor III

Dear. Support teams

I'm trying to control ISELED using the [iseled_freemaster_s32k144] example. Although controlling ISELED through digLED_Set functions has been successful, there is a problem with receiving ISELED responses through digLED_Read functions. In addition, ISELED's response to the digLED_Init_Strip function is also "RECEPTION_TIMEOUT". When the digLED_Read functions are called in this state, abnormal values are stored in the result buffer, and ISELED's response is "CHAINLENGTH_ERROR". How should I solve this situation? Please refer to the attached materials.

**Environment

RTM ver: 3.0.0

ISELED Driver ver: 3.0.0

IDE: S32DS for ARM v2.2

Best regards.

when_call_digLED_Read_PWM_Blue.png

0 Kudos
Reply
0 Replies