Error occurred while connecting to the interface hardware or target

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error occurred while connecting to the interface hardware or target

Jump to solution
3,142 Views
Anilpatil_SasvaAuto
Contributor III

Hello Team,

I am using S32K144EVB and tried to run a sample application(hello_world_s32k118) with PE micro debugger (built-in OpenSDA) to check if the EVB is fine. Things were not going well and got errors as below.

Anilpatil_SasvaAuto_0-1715345747182.png

Anilpatil_SasvaAuto_1-1715345758763.png

Please provide the solution ASAP

0 Kudos
Reply
1 Solution
3,037 Views
Anilpatil_SasvaAuto
Contributor III
It is working now, the issue is with the power supply. need to change J107 for USB supply
Thanks for the support.

View solution in original post

7 Replies
3,049 Views
Anilpatil_SasvaAuto
Contributor III

Hello World code

0 Kudos
Reply
3,039 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Have you already referred to that link?
Please tell me which step does not meet expectations.
If you don't tell me in detail, I won't be able to help you solve this problem.

0 Kudos
Reply
3,038 Views
Anilpatil_SasvaAuto
Contributor III
It is working now, the issue is with the power supply. need to change J107 for USB supply
Thanks for the support.
3,117 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Since you are using S32K144EVB, why do you want to run a sample application(hello_world_s32k118)? Please run the S32K144 example in the future.

I happened to be discussing a similar issue with another customer, please refer to: S32K144 EVB Red led 계속 on 상태입니다.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,822 Views
Anilpatil_SasvaAuto
Contributor III
 
0 Kudos
Reply
3,109 Views
Anilpatil_SasvaAuto
Contributor III

Sorry, it's a copy mistake. I have run the S32K144 example.

Anilpatil_SasvaAuto_0-1715577432997.png

 

0 Kudos
Reply
3,103 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Which example codes do you loaded into the device? Any for CSEc?
Did you secure the device?(FSEC SEC=secured )

Doesn't P&E Recovery Utility halt MCU? Please tell me what problem occurred during the operation.

0 Kudos
Reply