Error in services launch sequence.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error in services launch sequence.

906 次查看
Faker
Contributor II

Hi Expert:

   I encounter a question in S32K166 device to debug or run example of LPUART. The Interface uses JTAG configured in debug configurations. With I pushing debug or run button, a dialog pops out that writes "Error in serices launch sequence, Starting J-Link GDB Server timed out".I don't know how to solve this problem,so I hope anyone here could help me. 

0 项奖励
2 回复数

895 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Faker,

There is a timeout value you can use for Launch the GDB server:
Please try to increase that zero value e.g. to 10, 100 or higher (I believe it it is in ms).

timeout.png
I hope this helps!

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励

882 次查看
Faker
Contributor II

Hi Robin,

   The probelm has been solved by a way that this chip which is secure need to be unsecured.

0 项奖励