Error configuring HWCOUNTER in S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error configuring HWCOUNTER in S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0

2,814 Views
Tmon
Contributor I

Hi, my configuration of the HWCOUNTER result in the following error:

"Error in external generator: 3104: The period and all the hardware timer parameters are not allowed together".

I have the S32K148 Evaluation board, and want to set the system HRUN to use PLL to reach 112MHz of the MCU and assigned FTM0 use PLL.

What is the criteria so that the period is allowed with the hardware?

The configurations and the error can are show in the attached pictures.

 

Tags (3)
0 Kudos
Reply
1 Reply

2,756 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Tmon 

Please note that the MCAL for S32K1xx devices is now considered legacy software. It is strongly recommended to transition to the newer RTDs (Real-Time Drivers for S32K1). For any further assistance or support, please reach out to your NXP representative. 

 

BR, VaneB

0 Kudos
Reply