Does the GPIO interrupt work in RUN mode?
ans: yes, when i set the port B0 low, the ISR works
Can you measure the power consumption at VDD or BUS_CLK at the CLKOUT pin to confirm the VLPS mode?
ans: the consumption before VLPS is >25mA, after set_McuMode, it is 10mA (but it is still high,which i measure that the consumption of MCU[without any software is 4mA])
Can you halt the MCU just before it enters the VLPS mode and check whether the interrups are not masked globaly and that NVIC is configured correctly?
ans: how to do it?
Please make sure the MCU does not enter the sleep-on-exit VLPS mode?
ans: MCU should not enter the sleep-on-exit ? but the RM said it should be, and i do configured that "sleep-on-exit" in MCU as below.

I find that after the set_McuMode(vlps), I set the PortB0 low, the PORT_CI_ICU_IP_B_EXT_IRQ_ISR works and it could turn on the light as well as the mcu mode is run. But I do not know how to make the program re_init all the modules. Or should I reset the mcu manually?