Hello all,
I have been using can_pal_s32k144 example from S32SDK_S321XX_RTM_4.0.1. In that example the CAN 0 instance is already enabled with flexible data in the peripheral setting as shown below.
Now i wanted an other CAN instance to be enabled for my application. So, i enabled a CAN 1 Instance in the same example project file with all the settings similar to the CAN 0 instance settings. But when i am trying to do this i couldn't able to enable the flexible data rate in the new instance CAN 1 as you can see below.
In this you can observe that the check box has been disabled by default. So, can you please help me with this.
What shouild i do to enable this CAN 1 instance simialr to that of CAN 0 instance which was set by the Example
#S32k144#
Solved! Go to Solution.
S32K144->Only FlexCAN0 support CAN FD feature.