EbTresos configure DET

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EbTresos configure DET

2,004 Views
mxdad
Contributor I

   when I Configuring Det Module,come with this question: "Module "Det_TS_T40D2M10I4R0" (defined in plugin "Det_TS_T40D2M10I4R0") defines the schema file "config/Det.xdm" which cannot be found (if the file is signed or crypted, it must be referenced in META-INF\CRYPTOMANIFEST.MF)." and Canif module also have this question,but other module has not this question!

  Please,how can I solved it?

 

0 Kudos
Reply
1 Reply

1,985 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @mxdad ,

The Det and CanIf is just a stub module(just for building process) in the NXP MCAL package. These modules will be provide by other company or third-party (Eg: Elektrobit, Vector, ....). So we do not provide the .xdm for these modules.

Best regards,

Hung

0 Kudos
Reply