Dubug with Cyclone in IAR for ARM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dubug with Cyclone in IAR for ARM

798件の閲覧回数
Raj_Nayyer
Contributor II

Hi,
I'm working with MCU S32K148 and I can Debug properly with PE_MultiLink Programmer but when I use Cyclone FX with the same cables (10Pin SWD) It says cant communicate with target.
for both case MCU is get power independently and I haven't use jumper in Cyclone.
What problem can it have.

Capture.PNG

0 件の賞賛
返信
1 返信

777件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

PORT A of Cyclone FX and PORT G of Multilink look the same.

PORTA CYCLONE FX PORTG Multilink.png

Have you installed the latest software and drivers for Cyclone FX?
Have you tried using other IDEs, for example, can S32DS be debugged with Cyclone FX?
By the way, Cyclone FX usage issues can submit a technical service request to PEMicro.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信