Does S32K144EVB-Q100 OpenSDA Serial port support send/receive break conditions?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does S32K144EVB-Q100 OpenSDA Serial port support send/receive break conditions?

跳至解决方案
1,049 次查看
PYGC
Contributor II

I want to use the opensda serial port to control S32K144EVB-Q100, and send break conditidion to re-initialize system.

0 项奖励
回复
1 解答
979 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @PYGC 

MK20, which is the MCU that has the OpenSDA FW and the S32K1 in terms of UART support:

S32K1 -> optional 13-bit break character generation / 11-bit break character detection and programmable 1-bit or 2-bit stop bits.

MK20 -> 13-bit break character option and 1 stop bit.

That said, it should be possible, but I do not guarantee functionality since it is not a functionality we offer.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,034 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @PYGC 

OpenSDA is a debugging/programming interface.

Could you explain what you mean by this part: "send break condition to re-initialize system"?

 

B.R.

VaneB

0 项奖励
回复
988 次查看
PYGC
Contributor II

What I mean is whether the virtual serial port on OpenSDA supports sending or receiving Break signal, Break is a continuous low level (> 12 bits of data).

Also the virtual serial port on the S32K144EVB does not seem to support two stop bits.

 

PYGC_0-1680596157522.png

 

0 项奖励
回复
980 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @PYGC 

MK20, which is the MCU that has the OpenSDA FW and the S32K1 in terms of UART support:

S32K1 -> optional 13-bit break character generation / 11-bit break character detection and programmable 1-bit or 2-bit stop bits.

MK20 -> 13-bit break character option and 1 stop bit.

That said, it should be possible, but I do not guarantee functionality since it is not a functionality we offer.

0 项奖励
回复
965 次查看
PYGC
Contributor II

OK, I tried but it didn't work, thank you.

 

0 项奖励
回复