Default boot mode and Boot pins in S32k142

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Default boot mode and Boot pins in S32k142

Jump to solution
689 Views
Jeevansagar
Contributor III

I am working on S32k142 MCU. I want the boot mode to be from Flash.

What is the default Boot Mode in S32k14x MCUs and also i did not found any Boot pins in the Pinout, How is the Boot mode configuration done?

thanks,

jeevan

Tags (1)
0 Kudos
Reply
1 Solution
675 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Jeevansagar 

S32K1xx devices have only one boot mode - from internal flash from address 0 (0x0 initial SP_main and 0x4 initial PC). There are no other options, so there are no boot pins.

Regards,

Lukas

 

 

 

 

 

 

 

View solution in original post

0 Kudos
Reply
1 Reply
676 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Jeevansagar 

S32K1xx devices have only one boot mode - from internal flash from address 0 (0x0 initial SP_main and 0x4 initial PC). There are no other options, so there are no boot pins.

Regards,

Lukas

 

 

 

 

 

 

 

0 Kudos
Reply