Critical inconsistency with S32K144 ADC_SC1x register between CPU specification and actual value

cancel
Showing results for 
Search instead for 
Did you mean: 

Critical inconsistency with S32K144 ADC_SC1x register between CPU specification and actual value

258 Views
Contributor II

There is a critical inconsistency identified between ADC specification and actual register value for ADC_SC1x.

 

Actual value in S32DS:

ADCH field only has 5 bits available and setting 0x1F disables it.1.png

These are the register values in memory window:

 2.png

 

CPU specification:

ADCH field has 6 bits available and setting 0x3F disables it, while 0x1F is a reserved value.

3.png

4.jpg

5.jpg

Hope NXP can clarify this issue. Which one is correct?

Labels (1)
Tags (3)
1 Reply

50 Views
NXP TechSupport
NXP TechSupport

Hi,

the register description is general across S32K1xx family. Some of the input channel options might not be available for
S32K144.

pastedImage_2.png

BR, Petr