hi
I want to input a signal from TRGMIX to eMIOS1_1.
So I set TRGMUX to the following:
TRGMUX eMIOS1_0 (eMIOS1_0) = 0x68 (LCU_0_LC3_out_i4)
But no signal is being input to eMIOS1_1.
The signal output from the LCU is fine.
The eMIOS1_1 input pin flag(UCIN) is not set either.
eMIOS is used to SAIC mode.
Please tell me the settings required to input a signal to eMIOS.
已解决! 转到解答。