Conflicting SDK driver files.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Conflicting SDK driver files.

1,016 Views
emb02
Contributor IV

Hello,

I have S32DS project I am using S32K144.

I am using S32 Design Studio for S32 Platform
Version: 3.5

When I am using config tools to generate peripheral, which gives the SDK that generate driver files but some driver files are already present in S32K144_SDK4.0.1 and that conflicting which gives multiple definition error. 

What will be the solution?

0 Kudos
Reply
1 Reply

991 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please use S32DS v3.4, it is mentioned in S32K1 SDK RTM 4.0.x release note.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply