Hello,
Now I have two projects.
S32K344 Project A was created based on RTD 1.0.0.
S32K344 Project B was created based on RTD 2.0.0.
RTD 1.0.0 and RTD 2.0.0 packages were both installed in DS32.
When I open project A, some Peripherals errors are displayed in CT(Config Tool), it seems DS32 using RTD 2.0.0 to load project.
My question is: is there any method that I can open project A without any error(load project by using RTD 1.0.0)?
PS: Uninstall RTD 2.0.0 can solve it but it's not conveniently.
Hi,
I guess no options is for that, maybe will be fixed in next release.
BR, Petr