Code is not executing after hard reset (S32K118)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code is not executing after hard reset (S32K118)

2,692件の閲覧回数
ambarishhundeka
Contributor III

Hello NXP Team,

We are using S32K118 controller in our project.

We are working on bootloader implementation.

We are using S32Design studio to build the project and lauterbach debugger is using for the flashing the application and debugging.

bootloader code is working fine in debug mode , but after hard reset code is not executing.

tried with toggling the LED with same configuration , still LED toggling code also not working after hard reset.

find the attached Example of LED blink code and please let us know the solution.

Thank you in Advance.

Regards,

Ambarish

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,381件の閲覧回数
ambarishhundeka
Contributor III

Hello,

Thank you for your reply .

Issue is resolved, problem with linker file.

Regards,

Ambarish

0 件の賞賛
返信

2,381件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Ambarish,

I tested your code and I find out a HardFault after MCU power off and power on.

On the below link I found information which could be helpful:

Debugging ARM Cortex-M0+ HardFaults | MCU on Eclipse 


However, also the linker file needs to be checked.

Best regards,

Diana

0 件の賞賛
返信